Ultrasonic Sensors FAQ

Open-Structure type, SMD type

Is there any difference of Max Input Voltage between Open-Structure and SMD type?

Difference of Max Input Voltage is as follows;


MA40S4S(Open):Square Wave, 40kHz, 10Vrms

MA40H1S(SMD):Square Wave, 40kHz, 6Vpp

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.
Send

For product inquiries, please contact us using our contact form.