PTC Thermistors (POSISTOR) FAQQ[PRG Series] What is the maximum voltage when two PRG series units are connected in parallel?

A

The maximum voltage does not change even if multiple POSISTORs are connected in parallel. Do not exceed the maximum voltage.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.