Murata announces the launch of 0402-size (1.0mm × 0.5mm) winding type inductors for audio line choke applications.
The popularization of smartphones has given rise to the problem of reduced audio quality due to the effects on the audio line of electromagnetic noise from the communication frequency bands. In response, Murata has developed a new series of 0402-size (1.0mm × 0.5mm) winding type inductors with excellent Z characteristics in the communication frequency bands (700MHz to 2,700MHz bands).
Murata Manufacturing Co., Ltd. is a worldwide leader in the design, manufacture and sale of ceramic-based passive electronic components & solutions, communication modules and power supply modules. Murata is committed to the development of advanced electronic materials and leading edge, multi-functional, high-density modules. The company has employees and manufacturing facilities throughout the world. For more information, visit Murata's website at www.murata.com