Jun Chié
Keysight Technologies Japan G.K. President and Representative Director Japan
Since its foundation in Silicon Valley, the electronic measurement business has always been the core business of Keysight for 76 years.
Anticipating a new era of network society, Keysight has promoted a comprehensive approach in its measurement business.
The election of cities in South Korea and Japan as the forthcoming Olympic Games hosts has driven Keysight to focus on the Asian market
The growing potential of 5G and IoT is greatly advancing Keysight’s accumulated core technologies to the next stage.
Let me talk about the measurement business. Measurement is the act of ascertaining that a product is made accurately in a manufacturing process. It is absolutely necessary when something new is born, that is, when technological innovation occurs. Keysight has contributed toward technological innovation in the fields of communications, defense, semiconductors, and computers. Keysight was spun off from Agilent Technologies, a life sciences and chemical analysis company, in 2014. Before that, Agilent was spun off from Hewlett Packard (HP) in 1999, bringing with it measurement, chemical analysis, and medical equipment and electronic component business, leaving HP with computer and printer business. HP, since 1939 when it was founded in Silicon Valley as a measurement equipment maker, had strengthened its presence primarily in the measurement business until the late 1960s. Keysight is a global company with a 76-year history of electronic measurement.
The measurement business is a low-profile business, but I think that it provides a basis for electronics and electric industries around the world. The development of the measurement business has always been along with the growth of these industries. HP was founded during the Second World War. HP has a history of developing its technologies in the field of military technology and equipment. Communication technologies have developed in this kind of environment, leading to the creation of demand in the private sector.
Keywords Are 5G and IoT
A New Era of Network Society
The globalization of communication technology and its application to everyday use have supported the growth of Keysight. For instance, the first mobile phones sold in the 1980s used to be only for those who could afford them because they were so expensive. The function was limited to transmission of voice, and the communication method, which was called cellular technology (WAN: wide area network) , differed by country. This technology was later digitized. In the 1990s, when PHS and PDC were adopted in Japan, gradual unification of communication standards began. Mobile phones today adopt a common global technology, which allows them to connect beyond borders. Furthermore, as the popularity of mobile phones increased, the price of each phone markedly decreased, allowing a greater number of ordinary people to own them. The greater the number of users, the more diversified the application. Mobiles phones were initially for transmission of voice; now they have become data communication terminals connected via the Internet, such as smartphones. To facilitate the data communication, communication technologies have evolved into such various forms as wireless LAN, besides cellular technology.
Communications connects everything: from equipment in automobiles to healthcare devices. Network is entering into a new era, and communication technologies have been reshaping their roles. In such an environment, measurement has been sought after as a means of effecting standardization or unification of various communication technologies.
We live in an era of transition, where we have begun to see a new trend of communications. For instance, what is envisioned by the 5G and IoT technologies is a world connecting everything around us, in which independent developments will evolve into those with greater relationship.
We have now been connected via Wi-Fi® and Bluetooth® technologies. Furthermore, there is a trend of further enhanced connection that is trying to connect more and different things. The amount of data traffic is about to surge. To cater to such an expected increase, the data traffic will speed up, and the bandwidth will increase and become multiplexed via optical fiber networks or wireless communications in the millimeter wave band called WiGig. Sufficiently high data communication speed will help cloud computing evolve further, which will make data processing or storage at each terminal device no longer necessary.
Reflecting the above-mentioned trend, demand in the measurement business has shifted to new measurement technologies such as millimeter-wave and ultra-wide band analysis, high-throughput measurement technologies for a great number of devices, and network optimization technologies.
History of Keysight
Keysight’s electronic measurement business dates back to the foundation of Hewlett-Packard (HP) in 1939. The startup electronic measurement business of HP, a now famous computer hardware equipment maker, was spun off from HP as Agilent in 1999. Fifteen years later, Keysight was spun off from Agilent.
【Company History】
1939 |
Bill Hewlett and Dave Packard founded an electronic measurement equipment company Hewlett-Packard in Palo Alto, California, USA. |
1999 |
Agilent Technologies was spun off from Hewlett-Packard. The entire business segment other than computing and printing (electronic measurement, chemical analysis, and medical equipment, and electronic components) was transferred to the new company. |
2000 |
Agilent Technologies becomes a fully independent company, following HP’s disposal of its Agilent shares. |
2001 |
Agilent sold its medical equipment unit to Philips. |
2005 |
Agilent spun off its electronic component unit, which became Avago Technologies. |
2006 |
Agilent spun off its semiconductor test unit, which became Verigy Ltd. |
2009 |
Agilent announced the purchase of Varian, Inc. for 1.5 billion U.S. dollars. |
2013 |
Agilent announced that it would split itself into two independent companies in 2014: Agilent Technologies would take control of the life sciences business unit, and Keysight Technologies would take over the electronic measurement equipment business unit. |
【Keysight’s Business Field】
Fields of Business
- Electronic component and communications field
- Aerospace and defense field
- Industrial equipment, computer, and semiconductor field
Products and Services
- The development and marketing of electronic measurement equipment (oscilloscopes, reference signal generators, spectrum analyzers, network analyzers, portable measurement equipment, etc.)
- The development and marketing of software programs (simulation software, analytical software, etc.)
- Customized solutions and consulting services in measurement
Expectations for the Asian Market
The Olympic Games in Japan and South Korea Will Be the Focus
5G is an ambitious next-generation technology, which conflates technologies thus far accumulated up to 4G and a fundamentally different new technology. 5G will have to deal with a range of millimeter waves such as 60 GHz, 70 GHz, and 80 GHz, where our common sense in the range of thus-far widely-used radio waves does not work. 5G, whilst posing this kind of technological challenge, promises various new opportunities: For example, 5G will realize ultra-high-speed, low- latency, and highly-reliable networks anywhere. When the communication methods were largely divided into CDMA and GSM, the CDMA system, which was mainly adopted in Japan and South Korea, was technologically superior to the GSM system, which was the most popular and successful globally. I personally believe that Asian countries, such as Japan and South Korea, will be a vanguard in the development of 5G network technologies. In the day of CDMA and GSM, it was a little too early to have a single unified communications standard, whereas today it is a time for a single unified standard to connect every corner of the globe. In particular, I think that two Olympic Games in Asia, namely, the 2018 Winter Olympics in Pyeongchang, South Korea and the 2020 Summer Olympics in Tokyo, will bring about a new era of communications in Asia.
The essence of IoT is to connect everything. Communication technologies for IoT do not need to be something new to be developed; already-existing popular technologies can be exploited. But, for each thing to be connected, a large number of various additional components, such as communication modules, will be necessary. An increase in the number of components is a great opportunity for business. That said, the usability, reliability, and user-interface are also important factors. How can measurement support mass-production of these kinds of communication modules or other components? This is the mission of Keysight.
Communication technologies have already become essential to new areas that had thus far had nothing to do with the technologies; these new areas are connected to networks. For example, in the United States, farms are connected to networks, and the production there is remotely controlled. In Europe, carbon dioxide emitted from factories is consumed in photosynthesis under LED lights to grow tulips, etc. These kinds of efforts to promote agricultural productivity led by governments are called an agricultural revolution “smart agriculture.” I expect that clothing will also be connected to networks in the future as smart fabrics. In this connection, China, India, and South East Asia, where the population grows rapidly, are markets that have the potential to be cultivated. Although business models in the new areas of business have not been established, there are many business chances today for parts manufacturers who are capable of miniaturizing and mass-producing components.
Providing All the Know-How That We Have Collected
Startup of a Comprehensive Solution Business Based on Measurement
The scope of business of Keysight is also gradually changing. The measurement business has now evolved from just operations of taking measurements for data collection into a comprehensive business that provides measurement-based consulting or management services as well as solutions to clients’ business challenges. We certainly take measurements to collect data, but what is important in this new business model is how we analyze the data and how we utilize the results in the development and production phases as well as in the quality control of our clients’ products.
To be competitive in the global market, competitive cost is a necessary condition, but not sufficient; speed matters most. A challenge that is common to many companies is how fast they can launch new products under development. We do not want to take up the time of our clients to bother with measurement-related work. If our clients can let measurement equipment take care of what it is good at, that is, measurements and analyses, then our clients can spend their time (and focus their resources) on business within their core competencies. At Keysight, we consider it our duty to make good measurement equipment that has high precision and high accuracy and is able to process quickly at the same time. We will use all of our resources, that is, our best practices, global experiences, and know-how that we have accumulated thus far for decades as well as the portfolio of our software and hardware, to provide solutions to our clients through our consulting services.
Strategy Increasing Business Potential
Corporate Culture of Keysight and Murata
In a world where everything is connected, attention is directed to parts manufacturers that have product lineups in all fields of sensors, components, passive and active devices, such as Murata. I think that Murata is better positioned in the market as it has a large market share in all of the mentioned components and devices. To expand the field of business for the next generation, Murata did not hesitate to use M&A whenever necessary, which helped it expand its product portfolio. The growth of their corporate earnings has been impressive. Murata correctly analyses the served available market, or SAM, based on its past business records or existing markets, to implement strategies to expand the most promising business. Its corporate culture, which focuses on personal and community relationships, has seemingly propelled it into success as well.
Murata and Keysight have a similar corporate philosophy. The backbone of both companies is engineering, innovation, and technologies. Both value personal relationships. HP was founded in 1939, and Murata in 1944. Although located on the opposite sides on the globe, the two companies started business around the same time; both value relationships with clients, and adopt a user-oriented manufacturing policy. I think that it is important to have this kind of similar corporate culture to enjoy a good business partnership.
Along with future technological development, I think that the partnership between Murata and Keysight will also evolve. The number of components and modules for wireless communications will grow exponentially. We know what Murata wants: miniaturization of components and cost reduction in manufacturing while the reliability of products is maintained. Will close collaboration in product development stages contribute toward improving the reliability of products? How can Keysight contribute toward the business of Murata? I think that we are about to enter into a new era.
Smart Agriculture and Smart Fabrics
【Smart Agriculture in the Netherlands】
The land area of the Netherlands is one fiftieth of that of Japan, and the arable land of the Netherlands is one fourth of that of Japan. The Netherlands has many cloudy days; so, fewer sunshine hours, resulting in lower temperatures throughout the year. The farm worker population in the Netherlands is less than one seventh of that of Japan. However, the Netherlands now has the world’s second largest agricultural industry.
The Dutch agricultural industry exports 68 billion in U.S. dollars, which is about thirty times larger than the Japanese agricultural export and the second largest in the world after the United States. The Dutch agricultural industry has made the world’s largest profit of 25 billion U.S. dollars. What made this amazing success story of the Dutch agricultural industry is the concept of smart agriculture.
All kinds of information technologies are adopted in smart agriculture: For example, sensing technologies and IoT network technologies are used for the automatic control of temperature, humidity, and nutrients in plant factories (indoor vertical farming systems). Renewable energy is also used in the factories for energy conservation. Big data, constantly collected through these smart services, are analyzed over cloud computing resources for yet further evolution.
Reference:
https://www.change-makers.jp/post/10444
【Smart Fabrics】
IoT is about to be introduced in the management of human physiological conditions. There is a demand among people who want to reassess their lifestyles or improve their athletic performances to have their own biological data. To cater to such demand, functional fabric materials have already been developed. The materials allow users to monitor their biological data, such as heart rate and cardiogram, just by wearing them. The use of smartphone coupling application programs allows wearers to store the monitored data on a cloud database; later, the wearers will be able to have counseling based on the analysis of the stored data.
Already-developed fabric materials use film-like materials that may be used as electrodes or power distributors. The materials are thin and stretchable, so they are primarily marketed for sportswear. The materials are made by inserting electrically conductive paste between elastic resin films to make all of the materials look like a film. The materials are about 0.3 mm thick and made comfortable to wear. The elasticity of the materials is more than 100%, which is greater than that of human skin. The materials, attached inside the sportswear, detect electrical signals, such as those from the cardiac muscles, at the electrodes, which are then transmitted to smartphones, etc. via the embedded communication device, to monitor the heart rate of the wearers. The materials can measure the skin surface temperature, perspiration, and acceleration as well. Besides the monitoring of athletic activities, the purpose of the materials may include the prevention of drowsy driving, in which the materials detect a driver’s sleepiness from the fluctuation of his or her monitored heart rate, the degree of relaxation of the wearer, etc.
Reference:
http://newswitch.jp/p/1678