Synthetic Quartz

History of Synthetic Quartz Crystals

In 1905, George Spezia (Italy) announced the growth of quartz crystal using hydrothermal method and it was the first report in the world about the hydrothermal growth of sizable quartz crystal. In Japan, Yamanashi University started the research work on the hydrothermal growth of quartz crystal in 1953. After the research and development, high temperature/pressure vessel called autoclave was improved, and growth-technique was also improved, and finally, the industrial production of synthetic quartz crystals was started in 1973 with the amount of 7 kg of crystals per one autoclave.

After the progress in crystal growth-technique, the quartz crystals having the same quality level of natural quartz crystals were able to be grown in mass production, and furthermore, upscale of autoclave was performed to increase the amount of crystals. In 1973, an autoclave with a capacity of 1 m3 was made and a full-fledged mass production was started. Now, an autoclave with a capacity of more than 4 m3 is under operation, and yield of quartz crystal per autoclave is above 2,000 kg.

Characteristics of Quartz Crystal

Characteristics of Quartz Crystal
Hardness: 7 (Mohs' hardness)
Specific gravity: 2.65 x 103 kg/m 3
Crystal system: Trigonal System
Chemical composition: SiO2
Relative permittivity: 4.5
Transition temperature: 573 degrees
Solubility: Soluble in fluorine compound

Piezoelectric effect

Since quartz crystal has piezoelectric property, applied force in some direction causes electrical charge. On the contrary, application of an electrical field across the quartz crystal causes deformation in the crystal. For instance, if a quartz crystal wafer which is perpendicular to X-axis (electric axis) is placed in an electric field as shown in the figure below, the wafer shrinks in X direction.

What is the growth of Synthetic Quartz Crystal?

Quartz crystal is grown using the phenomena that the solubility of quartz crystal in alkali-liquid is different at different temperature, and it is grown at high temperature under high-pressure. The vessel for growth is a pressure vessel called an autoclave. Raw material, many pieces of lasca (small piece of natural quartz crystal) , is placed in the lower part of autoclave and seeds are suspended in the upper part. Then the vessel is filled with water and mineralizer such as Na2CO3 or NaOH, and after encapsulating, it is heated up to gain high pressure. Finally, it reaches to supercritical state and the growth begins. By keeping the temperature of the upper part of autoclave lower than that of the lower part of autoclave, convection occurs and dissolved quartz crystal is moved from the lower part to the upper part, then the dissolved quartz crystal precipitates on the seed crystal. The synthetic quartz crystal is grown with the repetition of this cyclic movement. Growth condition, size and orientation of seed crystal are adjusted to produce the synthetic quartz crystals, which have different shape, dimensions and properties, for various applications. Since the synthetic quartz crystals are grown under strict control, they have controlled shape, dimensions and properties.

What is the seed crystal?

The orientation of seed crystal is determined considering the efficiency of production of quartz crystal unit. The synthetic quartz crystals grown using X-cut or r-cut seed are used to make thickness-share mode quartz crystal units for high frequency range application, and the contour-mode quartz crystal units for middle frequency range application. The synthetic quartz crystals grown using rotated X-cut seed are used to make extension or flexure-mode quartz crystal units for low frequency range application. In some cases, a thin layer, called seed veil, which consists of foreign object covers the seed in the grown crystal. And it deeply affects to the quality of quartz crystal.

Quality evaluation of synthetic quartz crystal

The amount of crystal defect and impurity in synthetic quartz crystal depends on growth rate, mineralizer and raw material. The growth rate affects greatly to the important properties such as infra-red absorption coefficient α, which correlates to Q value, and frequency –temperature characteristics. The larger growth rate causes increase in α, decrease in Q value, and dispersion in frequency-temperature characteristics. The quality index of synthetic quartz crystal was originally a Q value, and a 5 MHz quartz crystal unit operated in 5th overtone mode was used to obtain the Q value. But it required laborious work to fabricate the 5 MHz crystal unit, so the index had been changed to the coefficient α instead of the Q value.

Standard specification for synthetic quartz crystal

Twinning

There shall be no electrical or optical twinning in the usable region.

Strain

There shall be no strain contained both inside and surface of seed crystal as well as in a grown quartz crystal.

Cracks and fractures

There shall be no cracks, chippings or fractures in the usable region.

Inclusion density

The specification is in accordance with the IEC 60758.

Grade/size range µm Desities per cm3
10 to 30 30 to 70 70 to 100 > 100
I a 2 1 0 0
I b 3 2 1 1
I 6 4 2 2
II 9 5 4 3
III 12 8 6 4

Infra-red quality indication:

Grade Maxima Estimated Q values (x 106)
α3585
Aa 0.015 3.8
A 0.024 3.0
B 0.050 2.4
C 0.069 1.8
D 0.100 1.4
E 0.16 1.0

Etch channel density

Grade Maximum number ρ per cm 3
1 10
2 30
3 100
4 300
5 600

Tokyo Denpa guarantees the Grade 2 for all the products. The products of the Grade 1 are available upon request.

Seed orientation, dimensions and location:
Orientation: 0°00'±15'
Dimensions: 1.5 mm±0.5mm (along Z axis)
Location: Within the hatched area of 3 mm maximum centered as described in the figure below

Specification for lumbered quartz crystal

Angles:
Rotation angle of Z-surface around X-axis:
00°00'±30'
Rotation angle of X-surface around Y-axis:
00°00'±15'
Rotation angle of X-surface around Z-axis:
00°00'±15'
Dimensional tolerance:
±0.1 mm (along X or Z axis)
Surface roughness:
12.5µm (10-point average)
Specification for lumbered quartz crystal

Typical synthetic quartz crystal

Quartz crystal for SAW devices

Quartz crystal for SAW devices Specification:
Inclusion density: II or better
Infra-red quality indication: C or better
Etch channel density: 2 or better

Quartz crystal for miniature crystal units or filters

Quartz crystal for miniature crystal units or filters Specification:
Inclusion density: II or better
Infra-red quality indication: B or better
Etch channel density: 2 or better

Quartz crystal for SAW devices

Quartz crystal for SAW devices Specification:
Inclusion density: II or better
Infra-red quality indication: B or better
Etch channel density: 2 or better

Lumbered Synthetic Quartz Crystal

Lumbered Synthetic Quartz Crystal

Anglar deviation

X axis-rotation of reference Z surface 0° 00' ±30'
Y axis-rotation of reference - X surface 0° 00' ±15'
Z axis-rotation of reference - X surface 0° 00' ±15

Surface

Surface finish #80 for diamond tool.

Cracks and fractures

There shall be no cracks or fractures in the usable region.

Strain

There shall be no strain contained both inside and surface of seed crystal as well as in a grown quartz crystal.

Standard specifications

Type
Type
No.
Dimension (mm)
Etch
channel
density
JIS
Grade
α3585
Maxima
α
Inclusion
density
JIS
Grade
Orienta
tion of
theseed
(θ)
Remarks
X
Z
Y
±0.2
±0.2
±0.5
Pure
Z
PB-18 9.0 18.0 200 1 0.050 1a~II 0°00' Z bar
PB-19 9.5 19.0 200 1 0.050 1a~II 0°00' Z bar
PB-20 10.0 20.0 200 1 0.050 1a~II 0°00' Z bar
PB-23 23.0 18.0 185 1 0.050 1a~II 2°00' Seedless
PB-31 31.0 18.0 185 1 0.050 1a~II 2°00' Seedless
PB-38 65.0 38.0 185 1 0.050 1a~II 2°00' Wristwatch
PB-41 65.0 41.0 185 1 0.050 1a~II 2°00' Wrist watch
SB-02 53.0 46.0 200 1 0.050 1a~II 0° 00' 2-inch SAW
SB-03 76.0 65.0 200 1 0.069 1a~II 0° 00' 3-inch SAW
SB-04 100.0 85.0 200 1 0.069 1a~II 0° 00' 4-inch SAW

※Custom-made items that are not included in the list are also available upon request.

Standard specifications