Common mode choke coils /
Common mode noise filters

DL-PL Series

DL□/PL□/NFG/NFP series


Common Mode Choke Coils(CMCC) reduce the common mode noise that is problematic in differential transmission (examples: USB, HDMI and Mipi), balanced transmission, power supply lines, and audio lines.
They are ideal for suppressing common mode noise with frequencies ranging from several megahertz to several hundred megahertz with no adverse effect on the signals (upper cut-off frequency).
Products can also be searched by series lineup or application.

Murata Icon X Selection tools

  Common Mode Choke Coils/Common Mode Noise Filters
>>Search by lineup
>>Search by Automotive lineup

Common Mode Choke Coils/Common Mode Noise Filters
>>Search by part number


Common Mode Choke Coils/Common Mode Noise Filters
>>Search by application ( PDF )
…click following chart
*Click here for user manual of selection chart. >




Selection chart for common mode choke coils
for signal lines

For non automotive grade

 
 

For automotive grade

 
 



Selection chart for common mode choke coils
for power lines

Selection chart by rated current

For non automotive grade

   

For automotive grade

   

Selection chart by noise suppression frequency

  Under 5A   Over 5A

For non automotive grade

 
 

For automotive
Powertrain/safety

   

For automotive
Infotainment

 

Murata Icon X Selection guide

Common Mode Choke Coils/Common Mode Noise Filters
Key point in product selection
When taking measures to deal with the noise in high-speed differential transmission lines, it is important for the noise to be suppressed while maintaining the signal quality.
>>Click here for Details

Murata Icon X Examples of noise suppression using common mode choke coils

Common Mode Choke Coils/Common Mode Noise Filters PLT10H series
Noise suppression of no less than 6A backed up by exceptional quality and ready supply
>>Click here for Details

for automotive LANs Suppression of noise in CANs using common mode choke coils
For automotive LANs Suppression of noise in CANs using common mode choke coils
Introduce noise countermeasure example for CAN line which is used for automotive communication network.
>>Click here for Details

techdoc
Examples of actions taken to comply with the CISPR25 standard governing radio emissions (noise emitted) from devices mounted in vehicles
There are many kinds of problematic noise that are emitted from the devices installed in vehicles.
The examples of the actions taken to suppress noise described here deal with the noise that is radiated from the USB signal cables.
>>Click here for Details

コモンモードチョークコイル/コモンモードノイズフィルタ
Signal skew improved by common mode choke coils
Signal skew, which is a problem in differential transmission lines, can be improved by using common mode choke coils. Details of the effects achieved can be found below.
>>Click here for Details

コモンモードチョークコイル/コモンモードノイズフィルタ
Noise suppression effects of common mode choke coils in HDMI interfaces
Since HDMI interfaces are high speed, the signal quality will be impaired if regular normal mode filters are used, therefore, these filters cannot be used. Details of examples where noise can be suppressed using suitable common mode choke coils while maintaining the signal quality can be found below.
>>Click here for Details

Suppression of High Current Noise
- Noise suppression using PLT10H -

Do you have any problem with noise?
Noise suppression using PLT10H.

Murata Icon X Basic facts about common mode choke coils

Here are explanations on various topics about common mode choke coils from “What are common mode choke coils?” to “How our products can be used to best effect.”

Common mode choke coils

Common mode choke coils for signal lines

How to use common mode choke coils for power supply lines

Murata Icon X PDF catalog

 Here you can download our PDF catalog with details on our common mode choke coils.

  Click here for Details
 

Murata Icon X Other Links