Theme 3
Differential transmission is widely utilized for high-speed signal lines of noise countermeasures of recent electronic devices. This theme explains the reason for this, the noise that should be taken into consideration in the differential transmission line, and the suppression methods for the noise. This theme also explains the basis of the mixed S parameter, which represents the transmission characteristics of the differential transmission line, and the effect of these characteristics.
[Average time required for reading: approx.13 mins]