The sensor itself does not emit LED or other light but instead detects changes in the amount of infrared rays which occur when a person (object) with a different temperature than the surrounding environment moves. Because it detects temperature differences, it is suited to the detection of human bodies which have a body temperature.
Passive component…Because it operates when there is human movement (temperature change), the low consumption current (standby current) is a significant feature and strength.
Murata's strengths include the technology application of pyroelectric ceramics based on ceramic technologies cultivated by Murata over many years and the advantages of low variation.