Ultrasonic sensors work with targets of any material or color. They are able to detect objects made of transparent glass or acrylic. Nevertheless, the reflection rate will differ according to the characteristics of the reflection target.
Reflected waves cannot be measured while the receiver is receiving direct waves.
→Short distance limit
If an object is too far away, its reflected waves may be too weak to be measured.
→Long distance limit