Ultrasonic SensorsBasic knowledge of ultrasonic sensors: Properties of sound waves

Properties of sound waves

The propagation speed of sound waves differs depending on the medium. In addition, sound waves have properties of reflection and transmission related to the acoustic impedance of the medium.

The higher the elasticity the faster sound travels.

○Sound travels more quickly through solids than through liquids, and through liquids more quickly than through gases.
Speed of sound = elasticity ÷ density

The speed of sound when traveling through the air is affected by the temperature.

○C = 331.5 + 0.6T [m/s]
C: Speed of sound traveling through air, T: Temperature (°C)

The greater the difference in acoustic impedance between media, the greater the reflection. When there is little difference in acoustic impedance between media, transmission occurs.

○Acoustic impedance=ρ・C
ρ: Density of medium, C: Speed of sound traveling through medium

Speed of sound and acoustic impedance within a medium

Every object has its own characteristic acoustic impedance. Acoustic impedance is expressed as a numeric value indicating the ease of sound propagation. It can be calculated as density of medium × speed of sound traveling through medium.

Zo=ρc

Ultrasonic waves are reflected when the difference in acoustic impedance between media is large, and they are transmitted when the difference is small.
Murata ultrasonic sensors propagate ultrasonic waves through the air. Since there is a very large difference with the acoustic impedance of water ( 106 ), reflection occurs at the boundary surface.

Speed of sound and acoustic impedance within various media

Propagation medium Zo=ρc ρ(kg/m3) c(m/s)
Steel 39×106 7700 5000
Aluminum 14×106 2700 5200
Fused quartz 12×106 2700 4400
Water 1.44×106 1000 1440
Air 410 1.2 340

Zo: Acoustic impedance
ρ: Density
c: sound speed

Directionality, resolution, and frequency

Here we describe the directionality, resolution, and attenuation of ultrasonic waves with relation to frequency.

Directionality

The directionality of the ultrasonic sensor describes a cone shape radiating upward from the top surface, with directionality defined as −6 dB compared with the front surface sound pressure. The directionality is wide compared to optical sensors, and one of its features is that it becomes sharper the higher the frequency.

Resolution

The higher the frequency, the higher the resolution.

Attenuation

Attenuation increases as the frequency rises, and the range becomes shorter.