Thermistors (Temperature Sensors)What are Thermistors?

What are Thermistors??
Thermistors are an electronic component whose resistance changes with changes in temperature.

Thermally Sensitive Resistor

Thermistor

Murata has commercialized two types of Thermistors.

Two kinds of Thermistor

Swipe left or right to change screens View in landscape mode.
Type PTC Thermistor
Positive Temperature Coefficient
NTC Thermistor
Negative Temperature Coefficient
Basic Function It has almost flat resistance-temperature characteristics near room temperature, but the resistance increases logarithmically when the temperature exceeds a certain level (Curie point).
Murata was the first company in the world to commercialize it in 1961.
The resistance decreases logarithmically from low temperature to high temperature. Has a relatively accurate resistance deviation over the entire temperature range. Generally speaking, thermistor refer to NTC Thermistor.
R-T char.