Select your region & language

Digital Panel Meters FAQQWhy aren't absolute maximum input ratings specified?

A
Absolute maximum input levels are specified on our data sheets as the "Input Voltage Range" or simply "Input Range". This rating is the meter's maximum continuous operating level at the highest-rated operating temperature. In practical applications, momentarily exceeding the input range by 10% will not harm any of our 2-wire meters.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.