Digital Panel Meters FAQQHow is input polarity displayed?

A

DMS Series meters indicate negative input signals by turning ON a minus sign display-segment ("-") located to immediate left of the half- digit. Positive inputs are indicated by turning OFF the minus sign segment. For example, "-1234" is displayed for negative inputs, and "1234" for positive inputs. The minus sign is ON when IN HI (pin 11) is slightly more negative than IN LO (pin 12). Operation of the minus sign is automatic and can not be externally disabled by the user.
How is input polarity displayed?

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.