Inductors FAQ

Characteristics

I would like to know how to specify the rated current.

The value shows the maximum DC current which can continuously flow through the inductor.
If this value is exceeded, the heating value becomes excessive and the quality can not be guaranteed.
We also provide products with specified rated currents based on the changes of the inductance value, in addition to this specified generation of heat.
Refer to the specifications of each product for details.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.
Send

For product inquiries, please contact us using our contact form.