LoRa FAQQWhat is the physical interface on device to load firmware (first time)? Is it possible to flash firmware through PIN 23 and 24? Do we need to connect to other PINS?

A

When customers load our modem firmware to TypeABZ-078 for the first time, we recommend them to use SW interface with ST-Link.

Return to LoRa Module Page

Back to LoRa FAQ List

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.