Microblower FAQ

Precautions on Using

Can multiple microblowers be driven in parallel in a single drive circuit?

No, it is not recommended.
The driving frequency of the individual microblowers is different. When multiple microblowers are connected to single drive circuit, it will cause the characteristics to deteriorate because the microblowers operate at a frequency different than the optimal drive frequency.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.
Send

For product inquiries, please contact us using our contact form.