Acceleration Sensors FAQ

Characteristics

What is ratiometricity and ratiometric error?

Ratiometricity means that zero point and sensitivity are proportional to the supply voltage. If the supply voltage is fluctuating the output will also vary. The idea is that when using the same reference voltage for both the sensor and the measuring part (A/D-converter) , an error in the reference voltage is automatically compensated for.

Ratiometric error is the relative deviation (%) from the proportional behaviour described above, i.e. if the output voltage changes 3% at a supply voltage change of 5% we have a 2% ratiometric error.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.
Send

For product inquiries, please contact us using our contact form.