Acceleration Sensors FAQ

Characteristics

If the max accelerometer cross-axis sensitivity is ± 5%, what is the angle between the direction of measurement (z axis) and the primary axis of sensitivity?

± 5 % cross-axis sensitivity corresponds to approx. 2,8° mounting error. Angle between secondary axis (z-axis) and primary axis (x-axis) is 87,2°.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.
Send

For product inquiries, please contact us using our contact form.