AMR Sensors FAQ

Characteristics

How does the current consumption change based on the input voltage?

The input voltage and current consumption have a proportional relationship.
For example, the MRMS501A-001 identifies levels at 1.8V. At 1.8V, we have 3μA (typ), and so a current consumption operating at 3.5V, which is almost twice 1.8V, is about 6μA (typ).

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.
Send

For product inquiries, please contact us using our contact form.