AMR Sensors FAQQWhat is sensitivity?

A
The sensitivity is the strength of the magnetic force that turns on (or off) the AMR sensor.
The ON sensitivity (Hon) is the magnetic force that turns on the AMR sensor which was off with no or weak magnetic field, and the OFF sensitivity (Hoff) is the magnetic force that turns off the AMR sensor which was on with a strong magnetic field.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.