AMR Sensors FAQQWhat are the important points when installing Murata AMR sensors?

A
AMR sensors may appear with reduced sensitivity due to installation on the PCB at a slanted angle. The same applies when the PCB is mounted in the device. Check that the AMR sensors are placed in a horizontal orientation for prototypes and for mass production when needed. If you feel that sensor operation is not quite right, before removing from the board, use a microscope or other instrument to carefully check the sensor placement.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.