Inclinometers FAQQHow does the frequency response look for Murata Electronics Oy's inclinometers?

A
In the SCA61T series the -3dB point is at 18 ±10Hz, 20dB/dec roll off. Attenuation at 1Hz is approx. 0,1% In the CBxH1G parts in the SCA610 series the -3dB point is at 6 ±4Hz, 20dB/dec, giving an attenuation of approx. 5,6% at 1Hz.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.