Gyro Sensors FAQ

Characteristics

What is the difference between an accelerometer and an inclinometer?

Murata Electronics Oy's inclinometers and accelerometers are all based on the same MEMS capacitive measuring technology. Different product versions are optimized for different purposes, determined by the g-range in which they are going to be used. The maximum g-range of the inclinometers is earth's gravitation (approximately 1g) . Murata Electronics Oy's accelerometers measure low-g ranges of ±0.26g up to ±12 g.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.
Send

For product inquiries, please contact us using our contact form.