Inclinometers FAQ

Characteristics

Is it possible for user to compensate zero point temperature drift using built-in temperature sensor the readings of which are available through an SPI interface?

Yes, you can use the internal temperature sensor to do 2nd or 3rd degree compensation.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.
Send

For product inquiries, please contact us using our contact form.