Piezoelectric Sounders FAQQIs there any problem with using a Piezoelectric Sounder (External Drive Type) at a frequency other than that used to obtain the specified sound pressure level?

A
A piezoelectric sounder (external drive type) is designed to produce sound at a stable sound pressure when it is driven at the frequency used to obtain the specified sound pressure, however it will also produce sound at other frequencies as well. Consequently, it can produce not only a single sound but also melodies and other complex sounds, enabling it to be used in such applications as operation confirmation sounds, alarms, melodies and pseudo sounds.

However, there are cases in which the sound pressure level becomes very small depending upon the drive frequency, although this will also depend upon the frequency characteristics of sound pressure level of each product, so check and evaluate the product before using it.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.