Ceramic Resonators (CERALOCK) FAQQPlease explain the role of each component of the oscillation circuit.

A
Each circuit value has the following role:

the oscillation circuit

Rf: Feedback resistor

The feedback resistor determines the bias of the oscillation circuit. Generally, C-MOS IC uses 100k ohms to 10M ohms (normally, 1M ohms) feedback resistance, while TTL IC uses 1k ohms to 10k ohms (normally, 4.7k ohms) feedback resistance because of low I/O impedance. If the feedback resistance is too large, the amount of feedback will be reduced, making the operating point unstable. If the feedback resistance is too small, the gain will be reduced, or the current will be increased (Recently, most ICs intgrates the feedback resistor).

Rd: Damping resistor

Damping resistor and loading capacitors work as low-passfilter that can suppress abnormal harmonic oscillation by reducing the gain in the high frequency range. Also, the IC gain can be limited and CERALOCK properly match IC, unwanted ringing, overshoot and undershoot can be suppressed. In the kHz band, the damping resistance should be several kilo-ohms, and in the MHz band, it should be between tens ohms and hundreds ohms. The damping resistor is optional.

CL1/CL2: Loading capacitor

This parameter is the most important for determining the stability of the oscillation circuit. If the load capacitance is too small, the oscillating waveform will be distorted, resulting in unstable oscillation. If it is too large, oscillation may stop. When compared with the same IC, the oscillation circuit providing lower frequency needs larger capacitance.

Rb: Bias resistor

When the IC gain is too high, or when TTL or triple-stage buffered IC is used, the bias resistor can be used to change the bias point intentionally in order to reduce the IC gain or suppress unstable oscillation. C-MOS IC uses a bias resistor of 1M ohms to 10M ohms, while TTL uses a bias resistor of several kilo-ohms to 10 kilo-ohms.

Each constant varies depending on the IC and the CERALOCK being used. For details, contact Murata.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.