Ceramic Resonators (CERALOCK) FAQ

Characteristics

What are the meanings of the Marking?

They shows frequency marking and EIAJ Monthly Code. Please refer to the following figure.
Marking
CSTCR_G / CSTNR_G / CSTNE_G / CSTNE_V Series
*1:Frequency Marking
The following table shows typical examples of frequency marking.
Regarding other frequency, please refer to each specification or contact us.
Series Explanation Example
CSTCR_G/
CSTNR_G
We mark the second decimal place of the frequency without a decimal point. 6.000MHz→600
CSTNE_G We mark the first decimal place of the frequency without a decimal point.
But we replace number with the alphabet when the integer part of the frequency is a 2-digit. 10→X、11→Y、12→Z.
8.000MHz→80
10.000MHz→X0
CSTNE_V We mark the code as the frequency.There is no regularity.Please refer to specification of components. 20.000MHz→E
24.000MHz→J

*2:EIAJ Monthly Code
Marking code for manufacturing month & year
EIAJ Monthly Code
  Note) One cycle (A to z ) : Four years

Related FAQs
Most people who viewed this page also referred to the following pages.
Q.
Does CERALOCK have orientation?
Q.
Is there any problem if CERALOCK is mounted in opposite direction?
Q.
Why does frequency correlation occur when CERALOCK is mounted in opposite direction?

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.
Send

For product inquiries, please contact us using our contact form.