Ceramic Resonators (CERALOCK) FAQQAre there any points to be aware of when using CERALOCK?

A
The construction of CERALOCK is shown as below, and ceramic element is hold as a two durability beams. This element is a ceramic thin plate (<100μm), so that it may caused a crack in ceramic element (this crack will lead to no oscillation) when strong external stress is added.
Metal cap is fixed on the substrate by adhesive. So when strong external force is added to the metal cap, it may come off.
Please do not handle with a strong external force to the ceramic resonator (both body and metal cap).
Structure of ceramic resonator(CSTCR type, CSTCC type)

Note:Structural Drawings of  Timing Devices
Structure drawings are provided on our website "my Murata". 
"my Murata" requires registration for access, and can be found through the following link. (Entry is Free)
We hope that the utilization of "my Murata" is advantageous so we may innovate together !

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.