Example of Problem Solving for InductorsHow to Keep Efficiency through Miniaturization

The power supply efficiency can be maintained as much as possible by using Murata's power inductors with low AC loss (core loss), which affects the efficiency at high frequencies accompanying the downsizing of DC-DC converters.

How to Keep Efficiency through Miniaturization

Downsizing of DC-DC Converter Circuits

When the switching frequency increase in a DC-DC converter circuit, the L value required for the power inductor decreases therefore, the overall DC-DC converter circuit can be downsized.

Downsizing of DC-DC Converter Circuits

The efficiency of a DC-DC converter can be improved by using an inductor with the largest possible inductance value and low AC loss (core loss) at the time of low current operation (PFM) , such as during standby.

Downsizing of DC-DC Converter Circuits

Keep in mind that there are frequency characteristics in the AC loss. Murata's ferrite multilayer inductors are excellent in low AC loss (core loss) characteristics, particularly at high frequencies, therefore improvement in efficiency can be expected.

Downsizing of DC-DC Converter Circuits

Example: In a switching frequency of 3 - 5 MHz, low AC loss (core loss) was achieved in a commonly used power inductor of about 1 uH.

For this reason, the power supply efficiency can be maintained as much as possible by using Murata's power inductors with low AC loss (core loss), which affects the efficiency at high frequencies accompanying the downsizing of DC-DC converters.

Other Examples

RF Inductors
Proposal of the Loss Reduction in the RF Circuit

The loss of the RF circuit depends on Q of the inductor to use for matching circuit. Here we propose the most suitable product to reduce the loss in the RF circuit.

RF Inductors Proposal of the Loss Reduction in the RF Circuit

RF Inductors
Proposal of the base exclusive possession area reduction by small size, the high-performance LQP03_02 series

Due to the high functionality and multiple bands of smart phones developed in recent years, the required number of high frequency inductors per unit has continued to increase.
We have introduced the miniature and highly functional LQP03_02 series for customers who are evaluating reduction of the design's package size and profile.

RF Inductors Proposal of the base exclusive possession area reduction by small size, the high-performance LQP03_02 series

RF Inductors
Proposal of the Noise Suppression Technology in the PA and Power Line -Example of Using Power Inductors for Chokes-

The noise suppression method of portable terminal PA and power-supply line for improvement of out-of-band unnecessary radiant.

RF Inductors Proposal of the Noise Suppression Technology in the PA and Power Line -Example of Using Power Inductors for Chokes-