Sound Components (Buzzer)Mechanism of sound

Mechanism and Principles of Piezoelectric Sound Components

What Is a Piezoelectric Diaphragm?

A piezoelectric diaphragm is a device for which a piezoelectric element with electrodes is bonded to a metal plate such as brass or nickel.

Image of Diaphragm

Structure of piezoelectric diaphragm

Piezoelectric sound components necessary have piezoelectric diaphragms.
This is a simple structure which a piezoelectric ceramic is adhered to a metal plate of brass or nickel-alloy.

Image of Structure of piezoelectric diaphragm

Mechanism of producing sound for piezo diaphragms

When a voltage is applied across the piezoelectric ceramics, it stretches in its plane. When a voltage is applied to piezoelectric diaphragm, as the metal plate does not stretch, it bends as shown in Fig (a).
When the polarity of the applied voltage is reversed, the piezoelectric ceramics shrinks and the metal plate bends toward the opposite side as shown in Fig (b).
When the direction of applied voltage changes alternately, the state of Fig (a) and Fig (b) is repeated as shown in Fig (c), producing sound waves in the air.

Mechanism of producing sound for piezo diaphragms (Figure a・b・c)

Function of a case

You can get higher sound by using the resonance effect when a product is case type.

(1) The peak of sound pressure level of diaphragm

Figure 1 of The peak of sound pressure level

(2) The peak of sound pressure level of amplified in a case

Figure 2 of The peak of sound pressure level

(3) 10 to 20 dB higher sound pressure level by resonance effect

Figure 3 of The peak of sound pressure level

By designing fosc and fcav close each other, you will get 10 to 20 dB higher sound pressure level compared to non-cased diaphragm.

Supplement
fo (resonance frequency)
Frequency at which a diaphragm resonates most efficiently
fcav (sound frequency)
Sound frequency in the case determined by the volume of the case and the dimensions of the hole that produces the sound (sound emitting hole)

Mechanism of Piezoelectric Buzzers

A piezoelectric buzzer has a structure in which a piezoelectric diaphragm and drive circuit are embedded into a case.
A single-frequency sound is generated with the input of a DC voltage into the drive circuit. This has a single tone.

Image of Piezoelectric Buzzers

Mechanism of Piezoelectric Sounders

A piezoelectric sounder has a structure in which a piezoelectric diaphragm is embedded into a case.
There is no drive circuit in the product; instead, sound is generated with the input of an external AC voltage. The tone can be changed with the frequency of the AC voltage.

Image of Piezoelectric Sounders

Mechanism for Changing the Scale and Volume

Scale

The scale (frequency) of a piezoelectric buzzer is determined for each product. It cannot be changed.
It is possible to change the scale (frequency) according to the frequency of the AC voltage for a piezoelectric sounder. However, the volume varies depending on the frequency.

Volume

The volume of a piezoelectric buzzer/sounder can be increased by raising the input voltage. However, please note that the input voltage of the product has a rating.