Ceramic Capacitors FAQQWhy the color of the ceramic elements seems different even within the same product?

A

The color of the ceramic element seems different between the top, bottom, and sides due to the transparency degree of the internal electrode.
Process control fluctuation of the manufacturing process or element lot could also cause this difference.
Although there is a slight difference, it doesn’t affect characteristics or reliability. 

Example 1.
The color of the ceramic element seems different between the top, bottom, and sides due to the degree of transparency.

(Fig.1)

Example 2.
The color of the ceramic element seems different due to the process control fluctuation of the manufacturing process or the ceramic material lot.

(Fig.2)

<Reference FAQ>

>Q. What colors are multilayer ceramic capacitors?

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.