Silicon Capacitors FAQQWhat does BV or BDV refer to?

A
Dielectric breakdown is a phenomenon that occurs when voltage exceeding a certain value is applied to the insulation, causing it to break down, and to lose its insulating properties, thereby allowing current to flow.
The voltage level above which this phenomenon occurs is called the breakdown voltage (abbreviated BV or BDV).
Each silicon capacitor product has a specified breakdown voltage, indicated as BV.
For information on the relationship between BV (breakdown voltage, BDV) and recommended working voltage, please visit here
Related terms : Silicon Capacitor (Si-Cap), Silicon IPD (Si-IPD, Integrated Passive Device), Breakdown voltage (BV, BDV), rated voltage (RV), recommended voltage, working voltage, drive voltage, voltage tolerance, withstanding tolerance

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.