Digital Panel Meters FAQQWhat exactly is a "half-digit"?

A

When digital panel meters first appeared on the market the convention of using a full-scale display range of "000" to "1999" for 3½ digit meters and "0000" to "19999" for 4½ digit meters became an industry standard. And, for reasons still unknown to this writer, the leading left-most "1" (also referred to as the most significant digit, or MSD) became known as the infamous "half-digit". This half-digit represents the one-thousands digit on a 3½ digit meter and the ten-thousands digit on a 4½ digit meter.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.