LoRa FAQQWhat is the difference between CMWX1ZZABZ-078 and CMWX1ZZABZ-091?

A

In terms of the performance and the software, basically there is no difference between these two modules. The only difference is the Hardware Encryption for AES. 

CMWX1ZZABZ-078 carries this function, but CMWX1ZZABZ-091 does not. Besides, the price is the same for both modules.


PART NUMBER CMWX1ZZABZ-078 CMWX1ZZABZ-091
Chipset SEMTECH SX1276
ST MCU STM32L082 STM32L072
External Host MCU No
Frequency (MHz) 860 to 930
Secure Element No
Hardware AES-128bit Accelerator Yes No
Software Test Firmware
Availability (Status) In Mass Production

Return to LoRa Module Page

Back to LoRa FAQ List

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.