Infrared Sensors FAQ

Characterictics

How far is detection distance of Pyroelectric infrared sensor?

Since the detection distance changes by various conditions, it cannot be specified.
The detection distance changes by the following conditions.
(1) Sensitivity of the sensor itself
(2) Type of Fresnel lens (mirror)
(3) Circuit condition
(Amplification factor, frequency characteristic of the amplifier circuit, threshold of the comparator, etc.)
(4) Environment temperature
(5) Condition of the object (people)
(Moving speed, height of people, clothing, moving direction, etc.)

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.
Send

For product inquiries, please contact us using our contact form.