Sounders FAQ

Characteristics

Please tell me how to replace an Electromagnetic Buzzer with a Piezoelectric Sounder (External Drive Type).

A general drive circuit for an electromagnetic buzzer that does not have a built-in drive circuit is shown in Fig.1.
Example of a drive circuit for an electromagnetic buzzer
Fig.1 Example of a drive circuit for an electromagnetic buzzer

You cannot produce a sound from a piezoelectric sounder by simply replacing an electromagnetic buzzer with a piezoelectric sounder in this circuit. It is necessary to replace the diode (used for suppressing spike current) with a resistor as shown in Fig.2.

Example of a drive circuit for a piezoelectric sounder and a piezoelectric diaphragm (external drive type) in the case where a transistor circuit is used
Fig.2 Example of a drive circuit for a piezoelectric sounder

Because a piezoelectric sounder has high impedance and is also voltage-driven, it can be driven directly from an IC. Consequently, the configuration of the drive circuit itself can also be simplified.

Related FAQs

Most people who viewed this page also referred to the following pages.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.
Send

For product inquiries, please contact us using our contact form.