Sounders FAQ

Configurations Material

Location of hole in the top of each product is not fixed for PKMCS/PKLCS series. Is it a defect?

This is not a defect. The location of open hole is not specified.
The Open hole is located in one place of 4 corners.
4kHz (The item starting with PKLCS4) do not have a hole in the top.
PKMCS/PKLCS

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.
Send

For product inquiries, please contact us using our contact form.