The various characteristics of lead type ceramic capacitors can be displayed in graphs.
Impedance, ESR, reactance, Q, dielectric dissipation factor (tanδ), equivalent inductance, equivalent capacitance, transmission characteristics (S21), reflection characteristics (S11), DC bias characteristics, temperature characteristics, and ripple heat generation characteristics
* Some parts are not displayed.
In the graph, the characteristics can be compared easily, because the characteristics of multiple items can be overwritten.
* In the XY axis of the graph, the Linear/Log can be switched and the display range can be set.