Inductors FAQQIf a lower inductance is required, there is a method to create this by the board pattern. Will inductors with low inductance no longer be used in the future?

A
If the inductor is structured on the board, variations will occur in the performance due to the variations in the processing accuracy of the board, or the materials.  On the other hand, since all the inductors used as components are inspected at the time of shipment, variations in the performance is extremely low, and stable performance can be acquired.  For this reason, we believe that inductors used as components will continue to be used.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.