Ceramic Capacitors FAQ QWhat precautions for insulation resistance must be observed when using capacitors?

A

The specifications of chip multilayer ceramic capacitors only stipulate the insulation resistance lower limit value, and no sorting is performed to ensure that the insulation resistance characteristics fall within a specified upper and lower limit range.
Refer to the detailed spec sheet of each product regarding insulation resistance lower limit values (initial state and after reliability testing).

In addition, due to the design and characteristics of chip multilayer ceramic capacitors, their insulation resistance values may vary in different usage environments.

Therefore, when using chip multilayer ceramic capacitors in circuits whose operation could be affected by the insulation resistance*, you will need to consider in the design stage ways to avoid malfunctions or sensing errors caused by insulation resistance that is too high or too low.

* In applications such as circuits for monitoring battery voltages, if the design is such that the DC voltage is divided by the insulation resistance of a chip multilayer ceramic capacitor, the division ratio (the voltages at the two poles of the capacitor) will vary with changes in the insulation resistance value.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.