Ceramic Capacitors FAQQWhat is the Structure, Materials of Ceramic Capacitors?

A

The structure of the most basic type of capacitor for storing electricity consists of a dielectric sandwiched between two electrodes. A multilayer ceramic capacitor consists of multiple layers of this structure to enable storage of a greater charge.

To determine the raw materials of each part of a ceramic capacitor product (MLCC or lead type), refer to the Structure diagram, Materials chart page.
You can also access the same data from "Product data > Structure diagram, Materials chart" on the Product Details pageProduct details page
.

<Related Links>
Basics of capacitors [Lesson 3] How multilayer ceramic capacitors are made

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.