Silicon Capacitors FAQ

Mounting

Can aluminum wires be used for wire bonding?

Aluminum wires can be used if the electrode uses Al-finishing. With standard Au-finishing, it is recommended that you use gold wires.
For more details, please check the “Murata_Main_Assembly_reccomendations-April_2017” in the Assembly Note.