Digital Panel Meters FAQQWhat happens when the input goes below the minimum specified level?

A
The answer to this question is model dependent. LCD display models will normally continue to operate well below their specified minimum input levels, but the display's contrast will gradually diminish, and more importantly, the readout accuracy is no longer guaranteed.
For LED display models, the intensity of the display will diminish, but the readout will remain fairly accurate down to the level at which the display becomes so dim that it becomes unreadable. In applications in which the display is required to be totally off at times, be sure to drive the meter with components which bring the input signal all the way to zero.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.