Inductors FAQ

Characteristics

How do I select an RF inductor?

There are three ways to select a Murata inductor.
  1. Select by the product specifications
  2. Select from the product lineup
  3. Select by cross-referencing the industry product number

1. Select by the product specifications
①Check the application.
②Enter the required inductance value and product dimensions.
③Check that the rated current value is at or below the current flowing to the circuit being used.
④If there are Rdc and SRF limits, enter the limit information.

Inductor_Chip_FAQ_Char_9-1


2. Select from the product lineup

From the selection tool tab, select the application General (Small size), General (Large size), For Automotive.

Use the selection tool indicating the size and Q value to select the appropriate product lineup according to the allowable size and Q characteristics.
After selecting a product lineup, select the required inductance value.
Check that the rated current value of the selected inductance value is at or below the current flowing to the circuit being used.

3. Select by cross-referencing a competitor’s product number

Enter a competitor’s product number to search for the corresponding Murata product number.

For possible problems when replacing competitor's product , see below.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.
Send

For product inquiries, please contact us using our contact form.