LoRa FAQQWhat is the difference between LoRa and FSK? Can we use both FSK (Frequency Shift Keying) and LoRa modulation?

A

Yes, it is possible to switch between FSK and LoRA via SPI register write.

Return to LoRa Module Page

Back to LoRa FAQ List

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.