Infrared Sensors FAQQIs a pyroelectric infrared sensor influenced by the air flow from heaters and air conditioners?

A
Yes, it is influenced.
When air blows on the pyroelectric infrared sensor, a sudden temperature change occurs on the surface of the sensor and the pyroelectric ceramic reacts to the temperature change, and an output may occur.
For this reason, use in a location where it is not influenced by air flow (no direct air flow).

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.