Diaphragm FAQ

Characteristics

Please tell me the maximum input voltage that can be applied to a Diaphragm.

Regarding a piezoelectric diaphragm, basically the maximum input voltage is not specified. The maximum input voltage to a piezoelectric diaphragm is affected by the specifications and fixing method of the product, and also by the frequency, and so on, of the input signal. In the case of a typical product listed in the catalog, generally a voltage of around 30 Vp-p can be applied without problem.