Piezoelectric Diaphragms FAQQPlease tell me the maximum input voltage that can be applied to a Diaphragm.

A
Regarding a piezoelectric diaphragm, basically the maximum input voltage is not specified. The maximum input voltage to a piezoelectric diaphragm is affected by the specifications and fixing method of the product, and also by the frequency, and so on, of the input signal. In the case of a typical product listed in the catalog, generally a voltage of around 30 Vp-p can be applied without problem.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.