Diaphragms FAQ

Configurations Material

What are the materials used in constructing Sound Components ?

The materials for components (ex.the terminal and plating) are located in the structure drawings, which are provided on our website "my Murata®". 
"my Murata®" requires registration for access, and can be found through the following link. https://my.murata.com/en/home (Entry is Free)

Structural Drawings of  Sound Components
* For information pertaining to the materials of SMD Type, please contact a local representative as this is not available on our website.

We hope that the utilization of "my Murata®" is advantageous so we may innovate together !