NTC Thermistors FAQQ[NC* Series] What is B constant?

A

This is the NTC thermistor constant calculated from the resistance of the two temperatures, and represents the rate of change of the resistance. We define in 2 points, 25°C and 50°C.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.